Continuous panel feed e-spool® flex 2.0

The e-spool flex 2.0 is the igus version of a cable drum without a slip ring. Cable diameters from 5mm  to 15mm can be used. The cable is always safely routed through a feed-through to ensure that it is wound up correctly.

Contents:
Order e-spool flex and e-spool flex mini now
The panel feed e-spool flex 2.0

Tech up

Tech up

  • Without interruption (no slip ring) also for energy,
    data, fluids and air
  • Space-saving
  • Can be fitted universally
  • Constant tensile strain on the cable
  • Locking mechanism of the cable
Cost down

Cost down

  • Cost-effective
  • Easy in case of repair
  • Simple replacement of the fitted cable, therefore adaptable
  • Four configuration levels adapted to  your requirement
Proof

Proof

Sustainability

Sustainability

  • No additional copper components in the system (apart from cable copper)
  • Parts are reusable
  • Less raw material required thanks to the option of partial repair instead of complete replacement
  • Have your energy chain recycled at the end of its life cycle with the igus Chainge recycling program . Irrespective of the manufacturer. You will receive a voucher for: chainge recycling program
  • igus has been an investor in Mura Technology from the beginning and is helping advance chemical recycling. From plastic waste to crude oil in 20 minutes.

Installation instructions

The illustrated assembly aid enables you to assemble the e-spool flex 2.0 and e-spool flex mini quickly and professionally.
This is how the e-spool flex is assembled.
This is how the e-spool flex mini is installed

Drive options e-spool flex

e-spool flex 2.0 with hand crank Version H: with hand crank
Cable diameter: from 5 to 15mm
Extension length: ≤15m
Order now!
e-spool flex 2.0 with retaining spring and locking function Version SP: with retaining spring and locking function
Cable diameter: from 5 to 15mm
Extension length: ≤15m
Order now!
e-spool flex 2.0 with retaining spring, locking function, and retraction brake Version SB: with retaining spring, locking function, and retraction brake.
Cable diameter: from 5 to 15mm | Extension length: ≤15m
Order now!

Drive options e-spool flex mini

e-spool flex mini with retaining spring and snap mechanism Version SP: with retaining spring and snap mechanism
Cable diameter: from 5 to 7mm
Extension length: ≤3m
Order now!
e-spool flex 2.0 with spring and ratchet lever Version SPL: with retaining spring and ratchet lever
Cable diameter: from 5 to 7mm
Extension length: ≤3m
Order now!
Note: Please consider VDE 0298 Part 5 (Current carrying capacity and conversion factors for wound cables) when selecting your cables and when using e-spool flex

NEW: e-spool flex accessories

Now with guide roller and brush attachment (optional)
e-spool flex brush attachment

Brush unit

Brush attachment for cleaning the cable before rolling it up.
e-spool flex guide roller

Guide roller

Idler pulley for "around the corner" extension.

Documentation

Documentation e-spool

Documentation cable drum e-spool flex

This documentation will provide you with all important information about e-spool flex - from technical data to hazard warnings to safety instructions.
Documentation e-spool mini

Documentation cable drum e-spool flex mini

This documentation will provide you with all important information about e-spool flex mini - from technical data to hazard warnings to safety instructions.

Structure of the e-spool flex 2.0


Discover the structure of the e-spool flex in the video.
e-spool® flex 2.0 Cables or hoses are inserted into the e-spool in a spiral pattern
e-spool® flex 2.0 The e-spool flex in detail from the inside (from left): housing, worm guide, cables/hoses, winding housing
e-spool® flex 2.0 The e-spool flex in detail from the outside (from left): housing, worm guide, cables/hoses, winding housing
e-spool® flex 2.0 Detail: cable/hoses inserted in the worm guide
e-spool® flex 2.0 Extension lengths up to 15m possible

Possible uses for the e-spool flex 2.0

e-spool flex on robots ... on industrial robots
e-spool flex in the car repair shop ... in the car repair shop
e-spool flex on platforms ... on platforms
e-spool flex in the harbour ... in harbours
e-spool flex in the warehouse ... in the warehouse

Possible uses of the e-spool flex mini

e-spool flex mini at the dentist's ... at the dentist's
e-spool flex mini at charging stations for e-bikes ... at charging stations for e-bikes
e-spool flex mini in the office ... in the office

e-spool flex

Tested in the igus laboratory

For the e-spool flex mini extension length

In its test laboratory, the largest in the industry, igus compared the e-spool flex mini with a competing product. The test evaluated the two products' extension lengths.

The results showed that the e-spool flex mini extension length was about three metres, while that of the competing product was only half that.

Consulting

I look forward to answering your questions

Shipping and consultation

In person:

Monday to Friday from 8:30 - 17:00.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH